Part Number: TMUXHS221
Other Parts Discussed in Thread: STRIKE
Hello,
I can see in the datasheet the absolute max Vio is 5.5V for a continuous voltage. In my application I will be using the mux as a 2:1 off of a USB C connector.
The block diagram would follow this sequence:
USB C Connector->ESD Protection->Over Voltage Protection Switch->Post Switch Clamp->TMUXHS221->AM64xx
In the event of short to VBUS, the OVP switch will kick in, but it still depends on the Post Switch Clamp. For approximately 60nS, the TMUXHS221 would see 7V, before the clamp activates fully.
Can the TMUXHS221 handle 60nS at 7V in a short to VBUS scenario?
Thank you,
Joe