Part Number: DP83869HM
I had Few Queries regarding this IC
1) As per datasheet its for media conversion - i want to use it for IG to 1G ethernet to optical media conversion
2) Can u do conversion Just by changing strap vales or does it require any Intellige device to set the registers of PHY or is both option available.
3) is 1.2V supported or do i need to give 1v only and can i use it without 1.8V.
4) i want to know how eaxctly media conversion can be implemented any ref circuits are available
Regards
Kushal N L