Part Number: TIC12400-Q1
Hi team,
I have some question about TIC12400-Q1.
It is assumed that one of the input signals is the wake-up source, and then successfully wakes up the MCU through INT. At this time, the MCU has woken up. Can I read which input signal wakes up through SPI?
Another question is, this is a 10-bit ADC acquisition, can the analog input be used as a wake-up source? For example, set a threshold, after exceeding this threshold, trigger the INT output, and then wake up the MCU