Part Number: DS160PR412
Other Parts Discussed in Thread: DS160PR410, DS160PR810
Hi,
Our project is using DS160PR412 as the redriver for our channel, there are couple questions about it:
1. For a rough estimation, how much IL budget the redriver is expected to extend?
2. For redriver pkg(both Tx and Rx) s parameters that included in IBIS AMI model folders, S21 and S12 are quite different, S12 and S22 are ~-300dB, which doesn't make sense. Please help to check.

3. For redriver, Rx IBIS AMI model is not auto adaptive, meaning during the simulation, I have to manually pick some values for each EQ parameter. If adding parameters from overall channel Tx and Rx EQ parameters, that will be a huge number to sweep. Just wondering if there will be any plan to update the redriver pkg and IBIS AMI models?
Thanks,
Qian