This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB926Q-Q1:Maximum number of I2C connections

Part Number: DS90UB926Q-Q1

Hi team,

I want to use the deserializer board as an I2C master to control devices on the serializer board.
How many devices can be controlled?
Is it theoretically possible to connect up to 112 nodes of the I2C standard?

Best,
Ryu.

  • Hi Ryu,

    How many devices can be controlled?

    Up to eight peripheral devices can be controlled by the 926.

    Is it theoretically possible to connect up to 112 nodes of the I2C standard?

    In theory, yes. In practice, however, the number of node connections is limited by the total bus capacitance of 400 pF. Would you be able to provide me with more details about your design and what you are looking to accomplish?

    Best,

    Nikolas