Part Number: TDES960
Hi Support Team
According to 7.4.19 CSI-2 Transmitter Frequency, it is stated that the CSI-2 timing parameters are automatically set when CSI-2 TX Data Rate=800Mbps and 1.6Gbps are set.
I believe that the CSI-2 timing parameters are automatically set under the following conditions, is this correct?
REFCLK=23MHz, CSI_PLL_CTL[1:0]=10, CSI-2 TX Data Rate=736Mbps
REFCLK=26MHz, CSI_PLL_CTL[1:0]=10, CSI-2 TX Data Rate=832Mbps
The above conditions were not listed in Table 7-14.
Best regards.