Part Number: SN65LVDS93A
Hi,
The input clock spec. is below.
-Input clock period Tc : 7.4 ns ~100 ns
in the other words clock frequency = 10 MHz ~ 153 MHz
-High-level input clock pulse width duration : 0.4Tc ~ 0.6Tc
I am going to in clock at 40MHz from the controller, but the duty cycle is 30:70.
Will the device work fine?
I see no problem with it for the reason that
the minimum High-level input clock pulse width duration is 2.96 ns ( = 7.4 * 0.4 )
and my input clock pulse width duration is 7.5 ns, which is greater than the minimum value.