Part Number: TS3USB221A-Q1
Dear TI
I have question about TS3USB221A-Q1.
It is USB2.0 MUX IC therefor need 2 USB Line.
But We will use port 1:USB Line Port 2: UART Line(TX,RX).
Question 1) Is it possible concept? Could we use as 1 USB and 1 UART line MUX?
(UART Voltage 1.8V or 3.3V)

Question2) If we didn't use low power mode (OE pin : high), How much consume the Current?
(VCC: high , S : High or Low)