Part Number: AM26C31
Other Parts Discussed in Thread: TPL7407LA
AM26C31について質問があります。
ラインドライバ出力トランジスタの耐電圧を教えてください。
同じGNDの制御ロジック24V回路を使用したいのですが。
ラインドライバ出力がオープンコレクタとして使用できることを教えてください。

お返事をお待ちしております。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The absolute maximum ratings do not allow 24 V. And there is only a single enable control signal for all four drivers, so it is probably not possible to get proper open-drain signals.
Why do you want to use the AM26C31 for this? Do you also need differential outputs? A plain driver like the TPL7407LA would work better for open-drain outputs.
Hi yoneyama,
Clemens is correct - this device cannot stand 24V on its bus pins (+/-14V is differential voltage max). Also due to device architecture its not really possible to mimic an open-drain system (from an internal architecture they are push-pull -not open drain; you'd need to use the enable + bus biasing resistors to mimic an open drain - but as Clemens alluded to there is only 1 enable for 4 different channels - so a true "open drain" style of operation is not possible)
Since this is single ended it seems as well I don't think RS-422 are the best type of devices - using a standard Driver like Clemens suggested would be a better place to start as I don't think the AM device will be a good fit for this application.
Best,
Parker Dodson