Part Number: TPD3S713-Q1
Dear Sir:
Regarding the TPD3S713-Q1 Design Issue.
There are some questions as below.
Please check to reply us asap.
Thanks a lot.
B.R
Vincent
The TPD3S713-Q1 is used on the End Equipment ( Navigation Modules ) .
1. No use the VBUS USB connector
The voltage of BUS (PIN15 ,16) uses the other external power 5V Source.
Is it correct?
2.
2. The TPD3S713-Q1 is used on the End Equipment ( Navigation Modules ) .
It is client mode.
Is it correct?

3. The Client mode.
PIN9 (INT1) = Low, INT1 connects to pull down Resistor 10Kohm to GND. Is it OK?
PIN8 (ILIM_SEL) = Low, ILIM_SEL connects to pull down Resistor 10Kohm to GND.
Is it OK?

4. The Client mode.
PIN8 (ILIM_SEL) = Low.
PIN19 (ILIM_LO) : RILIM_LO = 80.6 Kohm , Is it OK?
PIN20 (ILIM_HI) : NC( NO CONNECTION) = Floating. Is it ok?