Part Number: SN65DSI83-Q1
Hi TI expert,
For the SN65DSI83-Q1, i see it is AEC-Q100 Qualified With the Following Results:– Device Temperature Grade 2: –40°C to +105°C Ambient Operating Temperature.
But in the 6.3 Recommended Operating Conditions, i see the maximum case temperature is 92.2°, which is quite lower than the 105°C Ambient Operating Temperature SN65DSI83-Q1 can support, could you please explain why the case temperature is lower than the Ambient Operating Temperature? As my understanding the case temperature shnould be higher than the ambient temperature, right?