This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB8044A: SMBus Mode

Part Number: TUSB8044A

Dear team, 

If we set SMBUSz to pull down when SMB us slave Operation, please review below operation and let me know your opinion. 

1. The host recognize 4 USB hub 0x44, 0x45, 0x46, 0x47h. is it normal operation? 

At datasheet like below, It seems normal for the host controller to recognize 44h, 45h and 46h. but what is 47h? 

2. If a customer modifies the device register value (00h to FFh) of one of the 0x44, 0x45, 0x46, 0x47h, does the other device value also change?

for example, when the customer modifies the device register value (00h to FFh) of 0x44 device, the register value of 0x45, 0x46, 0x47h is also changed. is it normal operation? 

Thank you.