Part Number: SN65HVD82
Other Parts Discussed in Thread: THVD1500, THVD1510
Hi team,
Could you please help check if we have new device with better cost and P2P for 5V RS485 to replace SN65HVD82?
Thanks,
Brian
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Brian,
So the THVD1510 is probably closest replacement - its pin to pin but has a few upgraded parameters - but it is a bit more expensive.
The THVD1500 as Clemens mentioned would be the most cost effective replacement, but that does come at a cost of worse ESD protection (HVD82 has and IEC 61000-4-2 contact rating of +/-12kV compared to the THVD1500 which has a rating of +/-8kV - the THVD1510 has +/-18kV if you need the higher ESD protection)
Please let me know if you have any other questions!
Best,
Parker Dodson