Hello,
I am doing a failure mode analysis for this driver that is on an interface card we use. So is it possible for LVDS250 driver to fault in such a way it would continually supply the 3.3V supply voltage to the receiver and would there be any current limiting or voltage limiting if this happened. I am only considering single point failures. In our situation we have an FPGA LVDS 2.5V supplied input buffer and don't want to destroy it if it gets 3.3V to the input. Also, the 100ohm termination on the receiver is internal so that could destroy the resistor and or the input buffer if the current is too high. It looks like in the datasheet the highest the output could be Vcm-max+1/2Vdiff-max ~1.8V. It looks like this driver can supply 27mA when shorted, which is quite a bit more than the older driver we used on a previous version of this interface card we are using.
Thanks,