This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24392: USB signal connection

Part Number: BQ24392

Hi, 

1) In BQ24392 datasheet it is specifically mentioned to use with micro/mini USB ports, will it work if it connected to type C port for power and USB2.0 signals?

2) Also in DP_HOST and DM_HOST pins can we connect USB device data lines, because in my application board will act as a device always and it should to connected to a host through the USB connector. In this case DP_CON and DM_CON will be the host. Kindly provide your thought on this.

Warm Regards,

Mythili B