Part Number: TCAN1044V
Hi team,
Could you help me understand why CAN protocol allows 11 "0"? based on my understanding, an additional "1" will be appended after 5"0"s, how can 11"0" achieve?

B&R
Lijia
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Lijia,
Thanks for reaching out, good question. When an error occurs, CAN controllers indicate this to the bus by deliberately transmitting 6 consecutive dominant ("0") bits on the bus to interrupt communication. These error frames can begin as soon as a node detects an error, including the transmitting node. One situation that could occur would be when the transmitting node detects an error that begins being signaled at the end of 5 consecutive dominant bits. This would require 6 more dominant bits to be sent, meaning 5 + 6 = 11 bits would need to be sent in a row.
You are correct that bit-stuffing causes CAN messages with 5 or more dominant "0" bits to have a recessive "1" bit stuffed into the data to prevent 6 consecutive dominants, but the exception is error frames, where this rule is deliberately violated in order to cause all nodes to interpret a communication error.
Best,
Danny