Part Number: TDES954
Other Parts Discussed in Thread: TSER953,
Hello:
Please provide reference design information for tdes954+tser953, which is a chip used for camera one to four conversion. Thank you!!!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
Thank you for your question. You can find system level and device level examples in the respective datasheets of these devices. For a detailed design example, please see section 8.2 of the datasheets. The TSER953 is a serializer, which will receive data from the camera. The TDES954 is a deserializer, which will receive the data from the serializer and then output to the system's processor/SOC/display. So for example, the high level flow of data would be camera->TSER953->TDES954->SOC, which is shown in the figure below. The TDES954 has two ports, allowing for data from two different cameras and TDES953s to be received. If you have additional questions, please let me know.

Regards,
Darrah