Part Number: DS90UB928Q-Q1
We are using UB928 to pair with UB927. We noticed that the IC on our board is very hot while the output image seems normal; we can hardly hold a finger on it, while the UB928 on OEM display is barely warm if at all. Please help us review the attached hardware design to see if any errors causing the issue. Another possibility is that the downstream IC (LT9211C) which connects to lvds output of UB928 is causing that?