This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TRS3232E: Question of RJ45 user case from TRS3232EIPWR

Part Number: TRS3232E


Hi Expert,

The customer is using the TRS3232EIPWR for console port, RJ45.

And the engineer is asking the concern of 100ohm on PIn A4,A5.

Pls see the schematic: 

Pls advice the concern of 100ohm and share us the reference design for this user case if had

Thanks

Eric

  • Hi Eric,

    I don't see any issue - unless I am missing something (please feel free to let me know if I am misunderstanding anything)  - those 100 Ohm resistors on A4/A5 aren't connected to the RS-232 signals on A6 and A3. If they are connected then yes - because you are overloading the RS-232 bus - but if they don't directly connect to the RS-232 bus I don't see an issue.

    Best,

    Parker Dodson