Part Number: DP83822I
There are some issues about driver reconciliation and register settings with DP83822I.
More detailed information will be added.
Could you help with it?
Thanks a lot.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DP83822I
There are some issues about driver reconciliation and register settings with DP83822I.
More detailed information will be added.
Could you help with it?
Thanks a lot.
Hi Chen,
We are not driver expert. But we do have some Linux driver reference for DP83822 hope this might help you on the driver issue.
// SPDX-License-Identifier: GPL-2.0
/* Driver for the Texas Instruments DP83822, DP83825 and DP83826 PHYs.
*
* Copyright (C) 2017 Texas Instruments Inc.
*/
#include <linux/ethtool.h>
#include <linux/etherdevice.h>
#include <linux/kernel.h>
#include <linux/mii.h>
#include <linux/module.h>
#include <linux/of.h>
#include <linux/phy.h>
#include <linux/netdevice.h>
#define DP83822_PHY_ID 0x2000a240
#define DP83825S_PHY_ID 0x2000a140
#define DP83825I_PHY_ID 0x2000a150
#define DP83825CM_PHY_ID 0x2000a160
#define DP83825CS_PHY_ID 0x2000a170
#define DP83826C_PHY_ID 0x2000a130
#define DP83826NC_PHY_ID 0x2000a110
#define DP83822_DEVADDR 0x1f
#define MII_DP83822_CTRL_2 0x0a
#define MII_DP83822_PHYSTS 0x10
#define MII_DP83822_PHYSCR 0x11
#define MII_DP83822_MISR1 0x12
#define MII_DP83822_MISR2 0x13
#define MII_DP83822_FCSCR 0x14
#define MII_DP83822_RCSR 0x17
#define MII_DP83822_RESET_CTRL 0x1f
#define MII_DP83822_GENCFG 0x465
#define MII_DP83822_SOR1 0x467
/* GENCFG */
#define DP83822_SIG_DET_LOW BIT(0)
/* Control Register 2 bits */
#define DP83822_FX_ENABLE BIT(14)
#define DP83822_HW_RESET BIT(15)
#define DP83822_SW_RESET BIT(14)
/* PHY STS bits */
#define DP83822_PHYSTS_DUPLEX BIT(2)
#define DP83822_PHYSTS_10 BIT(1)
#define DP83822_PHYSTS_LINK BIT(0)
/* PHYSCR Register Fields */
#define DP83822_PHYSCR_INT_OE BIT(0) /* Interrupt Output Enable */
#define DP83822_PHYSCR_INTEN BIT(1) /* Interrupt Enable */
/* MISR1 bits */
#define DP83822_RX_ERR_HF_INT_EN BIT(0)
#define DP83822_FALSE_CARRIER_HF_INT_EN BIT(1)
#define DP83822_ANEG_COMPLETE_INT_EN BIT(2)
#define DP83822_DUP_MODE_CHANGE_INT_EN BIT(3)
#define DP83822_SPEED_CHANGED_INT_EN BIT(4)
#define DP83822_LINK_STAT_INT_EN BIT(5)
#define DP83822_ENERGY_DET_INT_EN BIT(6)
#define DP83822_LINK_QUAL_INT_EN BIT(7)
/* MISR2 bits */
#define DP83822_JABBER_DET_INT_EN BIT(0)
#define DP83822_WOL_PKT_INT_EN BIT(1)
#define DP83822_SLEEP_MODE_INT_EN BIT(2)
#define DP83822_MDI_XOVER_INT_EN BIT(3)
#define DP83822_LB_FIFO_INT_EN BIT(4)
#define DP83822_PAGE_RX_INT_EN BIT(5)
#define DP83822_ANEG_ERR_INT_EN BIT(6)
#define DP83822_EEE_ERROR_CHANGE_INT_EN BIT(7)
/* INT_STAT1 bits */
#define DP83822_WOL_INT_EN BIT(4)
#define DP83822_WOL_INT_STAT BIT(12)
#define MII_DP83822_RXSOP1 0x04a5
#define MII_DP83822_RXSOP2 0x04a6
#define MII_DP83822_RXSOP3 0x04a7
/* WoL Registers */
#define MII_DP83822_WOL_CFG 0x04a0
#define MII_DP83822_WOL_STAT 0x04a1
#define MII_DP83822_WOL_DA1 0x04a2
#define MII_DP83822_WOL_DA2 0x04a3
#define MII_DP83822_WOL_DA3 0x04a4
/* WoL bits */
#define DP83822_WOL_MAGIC_EN BIT(0)
#define DP83822_WOL_SECURE_ON BIT(5)
#define DP83822_WOL_EN BIT(7)
#define DP83822_WOL_INDICATION_SEL BIT(8)
#define DP83822_WOL_CLR_INDICATION BIT(11)
/* RCSR bits */
#define DP83822_RGMII_MODE_EN BIT(9)
#define DP83822_RX_CLK_SHIFT BIT(12)
#define DP83822_TX_CLK_SHIFT BIT(11)
/* SOR1 mode */
#define DP83822_STRAP_MODE1 0
#define DP83822_STRAP_MODE2 BIT(0)
#define DP83822_STRAP_MODE3 BIT(1)
#define DP83822_STRAP_MODE4 GENMASK(1, 0)
#define DP83822_COL_STRAP_MASK GENMASK(11, 10)
#define DP83822_COL_SHIFT 10
#define DP83822_RX_ER_STR_MASK GENMASK(9, 8)
#define DP83822_RX_ER_SHIFT 8
#define MII_DP83822_FIBER_ADVERTISE (ADVERTISED_TP | ADVERTISED_MII | \
ADVERTISED_FIBRE | \
ADVERTISED_Pause | ADVERTISED_Asym_Pause)
struct dp83822_private {
bool fx_signal_det_low;
int fx_enabled;
u16 fx_sd_enable;
};
static int dp83822_set_wol(struct phy_device *phydev,
struct ethtool_wolinfo *wol)
{
struct net_device *ndev = phydev->attached_dev;
u16 value;
const u8 *mac;
if (wol->wolopts & (WAKE_MAGIC | WAKE_MAGICSECURE)) {
mac = (const u8 *)ndev->dev_addr;
if (!is_valid_ether_addr(mac))
return -EINVAL;
/* MAC addresses start with byte 5, but stored in mac[0].
* 822 PHYs store bytes 4|5, 2|3, 0|1
*/
phy_write_mmd(phydev, DP83822_DEVADDR, MII_DP83822_WOL_DA1,
(mac[1] << 8) | mac[0]);
phy_write_mmd(phydev, DP83822_DEVADDR, MII_DP83822_WOL_DA2,
(mac[3] << 8) | mac[2]);
phy_write_mmd(phydev, DP83822_DEVADDR, MII_DP83822_WOL_DA3,
(mac[5] << 8) | mac[4]);
value = phy_read_mmd(phydev, DP83822_DEVADDR,
MII_DP83822_WOL_CFG);
if (wol->wolopts & WAKE_MAGIC)
value |= DP83822_WOL_MAGIC_EN;
else
value &= ~DP83822_WOL_MAGIC_EN;
if (wol->wolopts & WAKE_MAGICSECURE) {
phy_write_mmd(phydev, DP83822_DEVADDR,
MII_DP83822_RXSOP1,
(wol->sopass[1] << 8) | wol->sopass[0]);
phy_write_mmd(phydev, DP83822_DEVADDR,
MII_DP83822_RXSOP2,
(wol->sopass[3] << 8) | wol->sopass[2]);
phy_write_mmd(phydev, DP83822_DEVADDR,
MII_DP83822_RXSOP3,
(wol->sopass[5] << 8) | wol->sopass[4]);
value |= DP83822_WOL_SECURE_ON;
} else {
value &= ~DP83822_WOL_SECURE_ON;
}
/* Clear any pending WoL interrupt */
phy_read(phydev, MII_DP83822_MISR2);
value |= DP83822_WOL_EN | DP83822_WOL_INDICATION_SEL |
DP83822_WOL_CLR_INDICATION;
return phy_write_mmd(phydev, DP83822_DEVADDR,
MII_DP83822_WOL_CFG, value);
} else {
return phy_clear_bits_mmd(phydev, DP83822_DEVADDR,
MII_DP83822_WOL_CFG, DP83822_WOL_EN);
}
}
static void dp83822_get_wol(struct phy_device *phydev,
struct ethtool_wolinfo *wol)
{
int value;
u16 sopass_val;
wol->supported = (WAKE_MAGIC | WAKE_MAGICSECURE);
wol->wolopts = 0;
value = phy_read_mmd(phydev, DP83822_DEVADDR, MII_DP83822_WOL_CFG);
if (value & DP83822_WOL_MAGIC_EN)
wol->wolopts |= WAKE_MAGIC;
if (value & DP83822_WOL_SECURE_ON) {
sopass_val = phy_read_mmd(phydev, DP83822_DEVADDR,
MII_DP83822_RXSOP1);
wol->sopass[0] = (sopass_val & 0xff);
wol->sopass[1] = (sopass_val >> 8);
sopass_val = phy_read_mmd(phydev, DP83822_DEVADDR,
MII_DP83822_RXSOP2);
wol->sopass[2] = (sopass_val & 0xff);
wol->sopass[3] = (sopass_val >> 8);
sopass_val = phy_read_mmd(phydev, DP83822_DEVADDR,
MII_DP83822_RXSOP3);
wol->sopass[4] = (sopass_val & 0xff);
wol->sopass[5] = (sopass_val >> 8);
wol->wolopts |= WAKE_MAGICSECURE;
}
/* WoL is not enabled so set wolopts to 0 */
if (!(value & DP83822_WOL_EN))
wol->wolopts = 0;
}
static int dp83822_config_intr(struct phy_device *phydev)
{
struct dp83822_private *dp83822 = phydev->priv;
int misr_status;
int physcr_status;
int err;
if (phydev->interrupts == PHY_INTERRUPT_ENABLED) {
misr_status = phy_read(phydev, MII_DP83822_MISR1);
if (misr_status < 0)
return misr_status;
misr_status |= (DP83822_LINK_STAT_INT_EN |
DP83822_ENERGY_DET_INT_EN |
DP83822_LINK_QUAL_INT_EN);
/* Private data pointer is NULL on DP83825/26 */
if (!dp83822 || !dp83822->fx_enabled)
misr_status |= DP83822_ANEG_COMPLETE_INT_EN |
DP83822_DUP_MODE_CHANGE_INT_EN |
DP83822_SPEED_CHANGED_INT_EN;
err = phy_write(phydev, MII_DP83822_MISR1, misr_status);
if (err < 0)
return err;
misr_status = phy_read(phydev, MII_DP83822_MISR2);
if (misr_status < 0)
return misr_status;
misr_status |= (DP83822_JABBER_DET_INT_EN |
DP83822_SLEEP_MODE_INT_EN |
DP83822_LB_FIFO_INT_EN |
DP83822_PAGE_RX_INT_EN |
DP83822_EEE_ERROR_CHANGE_INT_EN);
/* Private data pointer is NULL on DP83825/26 */
if (!dp83822 || !dp83822->fx_enabled)
misr_status |= DP83822_ANEG_ERR_INT_EN |
DP83822_WOL_PKT_INT_EN;
err = phy_write(phydev, MII_DP83822_MISR2, misr_status);
if (err < 0)
return err;
physcr_status = phy_read(phydev, MII_DP83822_PHYSCR);
if (physcr_status < 0)
return physcr_status;
physcr_status |= DP83822_PHYSCR_INT_OE | DP83822_PHYSCR_INTEN;
} else {
err = phy_write(phydev, MII_DP83822_MISR1, 0);
if (err < 0)
return err;
err = phy_write(phydev, MII_DP83822_MISR2, 0);
if (err < 0)
return err;
physcr_status = phy_read(phydev, MII_DP83822_PHYSCR);
if (physcr_status < 0)
return physcr_status;
physcr_status &= ~DP83822_PHYSCR_INTEN;
}
return phy_write(phydev, MII_DP83822_PHYSCR, physcr_status);
}
static irqreturn_t dp83822_handle_interrupt(struct phy_device *phydev)
{
bool trigger_machine = false;
int irq_status;
/* The MISR1 and MISR2 registers are holding the interrupt status in
* the upper half (15:8), while the lower half (7:0) is used for
* controlling the interrupt enable state of those individual interrupt
* sources. To determine the possible interrupt sources, just read the
* MISR* register and use it directly to know which interrupts have
* been enabled previously or not.
*/
irq_status = phy_read(phydev, MII_DP83822_MISR1);
if (irq_status < 0) {
phy_error(phydev);
return IRQ_NONE;
}
if (irq_status & ((irq_status & GENMASK(7, 0)) << 8))
trigger_machine = true;
irq_status = phy_read(phydev, MII_DP83822_MISR2);
if (irq_status < 0) {
phy_error(phydev);
return IRQ_NONE;
}
if (irq_status & ((irq_status & GENMASK(7, 0)) << 8))
trigger_machine = true;
if (!trigger_machine)
return IRQ_NONE;
phy_trigger_machine(phydev);
return IRQ_HANDLED;
}
static int dp8382x_disable_wol(struct phy_device *phydev)
{
return phy_clear_bits_mmd(phydev, DP83822_DEVADDR, MII_DP83822_WOL_CFG,
DP83822_WOL_EN | DP83822_WOL_MAGIC_EN |
DP83822_WOL_SECURE_ON);
}
static int dp83822_read_status(struct phy_device *phydev)
{
struct dp83822_private *dp83822 = phydev->priv;
int status = phy_read(phydev, MII_DP83822_PHYSTS);
int ctrl2;
int ret;
if (dp83822->fx_enabled) {
if (status & DP83822_PHYSTS_LINK) {
phydev->speed = SPEED_UNKNOWN;
phydev->duplex = DUPLEX_UNKNOWN;
} else {
ctrl2 = phy_read(phydev, MII_DP83822_CTRL_2);
if (ctrl2 < 0)
return ctrl2;
if (!(ctrl2 & DP83822_FX_ENABLE)) {
ret = phy_write(phydev, MII_DP83822_CTRL_2,
DP83822_FX_ENABLE | ctrl2);
if (ret < 0)
return ret;
}
}
}
ret = genphy_read_status(phydev);
if (ret)
return ret;
if (status < 0)
return status;
if (status & DP83822_PHYSTS_DUPLEX)
phydev->duplex = DUPLEX_FULL;
else
phydev->duplex = DUPLEX_HALF;
if (status & DP83822_PHYSTS_10)
phydev->speed = SPEED_10;
else
phydev->speed = SPEED_100;
return 0;
}
static int dp83822_config_init(struct phy_device *phydev)
{
struct dp83822_private *dp83822 = phydev->priv;
struct device *dev = &phydev->mdio.dev;
int rgmii_delay;
s32 rx_int_delay;
s32 tx_int_delay;
int err = 0;
int bmcr;
if (phy_interface_is_rgmii(phydev)) {
rx_int_delay = phy_get_internal_delay(phydev, dev, NULL, 0,
true);
if (rx_int_delay <= 0)
rgmii_delay = 0;
else
rgmii_delay = DP83822_RX_CLK_SHIFT;
tx_int_delay = phy_get_internal_delay(phydev, dev, NULL, 0,
false);
if (tx_int_delay <= 0)
rgmii_delay &= ~DP83822_TX_CLK_SHIFT;
else
rgmii_delay |= DP83822_TX_CLK_SHIFT;
if (rgmii_delay) {
err = phy_set_bits_mmd(phydev, DP83822_DEVADDR,
MII_DP83822_RCSR, rgmii_delay);
if (err)
return err;
}
phy_set_bits_mmd(phydev, DP83822_DEVADDR,
MII_DP83822_RCSR, DP83822_RGMII_MODE_EN);
} else {
phy_clear_bits_mmd(phydev, DP83822_DEVADDR,
MII_DP83822_RCSR, DP83822_RGMII_MODE_EN);
}
if (dp83822->fx_enabled) {
err = phy_modify(phydev, MII_DP83822_CTRL_2,
DP83822_FX_ENABLE, 1);
if (err < 0)
return err;
/* Only allow advertising what this PHY supports */
linkmode_and(phydev->advertising, phydev->advertising,
phydev->supported);
linkmode_set_bit(ETHTOOL_LINK_MODE_FIBRE_BIT,
phydev->supported);
linkmode_set_bit(ETHTOOL_LINK_MODE_FIBRE_BIT,
phydev->advertising);
linkmode_set_bit(ETHTOOL_LINK_MODE_100baseFX_Full_BIT,
phydev->supported);
linkmode_set_bit(ETHTOOL_LINK_MODE_100baseFX_Half_BIT,
phydev->supported);
linkmode_set_bit(ETHTOOL_LINK_MODE_100baseFX_Full_BIT,
phydev->advertising);
linkmode_set_bit(ETHTOOL_LINK_MODE_100baseFX_Half_BIT,
phydev->advertising);
/* Auto neg is not supported in fiber mode */
bmcr = phy_read(phydev, MII_BMCR);
if (bmcr < 0)
return bmcr;
if (bmcr & BMCR_ANENABLE) {
err = phy_modify(phydev, MII_BMCR, BMCR_ANENABLE, 0);
if (err < 0)
return err;
}
phydev->autoneg = AUTONEG_DISABLE;
linkmode_clear_bit(ETHTOOL_LINK_MODE_Autoneg_BIT,
phydev->supported);
linkmode_clear_bit(ETHTOOL_LINK_MODE_Autoneg_BIT,
phydev->advertising);
/* Setup fiber advertisement */
err = phy_modify_changed(phydev, MII_ADVERTISE,
MII_DP83822_FIBER_ADVERTISE,
MII_DP83822_FIBER_ADVERTISE);
if (err < 0)
return err;
if (dp83822->fx_signal_det_low) {
err = phy_set_bits_mmd(phydev, DP83822_DEVADDR,
MII_DP83822_GENCFG,
DP83822_SIG_DET_LOW);
if (err)
return err;
}
}
return dp8382x_disable_wol(phydev);
}
static int dp8382x_config_init(struct phy_device *phydev)
{
return dp8382x_disable_wol(phydev);
}
static int dp83822_phy_reset(struct phy_device *phydev)
{
int err;
err = phy_write(phydev, MII_DP83822_RESET_CTRL, DP83822_SW_RESET);
if (err < 0)
return err;
return phydev->drv->config_init(phydev);
}
#ifdef CONFIG_OF_MDIO
static int dp83822_of_init(struct phy_device *phydev)
{
struct dp83822_private *dp83822 = phydev->priv;
struct device *dev = &phydev->mdio.dev;
/* Signal detection for the PHY is only enabled if the FX_EN and the
* SD_EN pins are strapped. Signal detection can only enabled if FX_EN
* is strapped otherwise signal detection is disabled for the PHY.
*/
if (dp83822->fx_enabled && dp83822->fx_sd_enable)
dp83822->fx_signal_det_low = device_property_present(dev,
"ti,link-loss-low");
if (!dp83822->fx_enabled)
dp83822->fx_enabled = device_property_present(dev,
"ti,fiber-mode");
return 0;
}
#else
static int dp83822_of_init(struct phy_device *phydev)
{
return 0;
}
#endif /* CONFIG_OF_MDIO */
static int dp83822_read_straps(struct phy_device *phydev)
{
struct dp83822_private *dp83822 = phydev->priv;
int fx_enabled, fx_sd_enable;
int val;
val = phy_read_mmd(phydev, DP83822_DEVADDR, MII_DP83822_SOR1);
if (val < 0)
return val;
phydev_dbg(phydev, "SOR1 strap register: 0x%04x\n", val);
fx_enabled = (val & DP83822_COL_STRAP_MASK) >> DP83822_COL_SHIFT;
if (fx_enabled == DP83822_STRAP_MODE2 ||
fx_enabled == DP83822_STRAP_MODE3)
dp83822->fx_enabled = 1;
if (dp83822->fx_enabled) {
fx_sd_enable = (val & DP83822_RX_ER_STR_MASK) >> DP83822_RX_ER_SHIFT;
if (fx_sd_enable == DP83822_STRAP_MODE3 ||
fx_sd_enable == DP83822_STRAP_MODE4)
dp83822->fx_sd_enable = 1;
}
return 0;
}
static int dp83822_probe(struct phy_device *phydev)
{
struct dp83822_private *dp83822;
int ret;
dp83822 = devm_kzalloc(&phydev->mdio.dev, sizeof(*dp83822),
GFP_KERNEL);
if (!dp83822)
return -ENOMEM;
phydev->priv = dp83822;
ret = dp83822_read_straps(phydev);
if (ret)
return ret;
dp83822_of_init(phydev);
if (dp83822->fx_enabled)
phydev->port = PORT_FIBRE;
return 0;
}
static int dp83822_suspend(struct phy_device *phydev)
{
int value;
value = phy_read_mmd(phydev, DP83822_DEVADDR, MII_DP83822_WOL_CFG);
if (!(value & DP83822_WOL_EN))
genphy_suspend(phydev);
return 0;
}
static int dp83822_resume(struct phy_device *phydev)
{
int value;
genphy_resume(phydev);
value = phy_read_mmd(phydev, DP83822_DEVADDR, MII_DP83822_WOL_CFG);
phy_write_mmd(phydev, DP83822_DEVADDR, MII_DP83822_WOL_CFG, value |
DP83822_WOL_CLR_INDICATION);
return 0;
}
#define DP83822_PHY_DRIVER(_id, _name) \
{ \
PHY_ID_MATCH_MODEL(_id), \
.name = (_name), \
/* PHY_BASIC_FEATURES */ \
.probe = dp83822_probe, \
.soft_reset = dp83822_phy_reset, \
.config_init = dp83822_config_init, \
.read_status = dp83822_read_status, \
.get_wol = dp83822_get_wol, \
.set_wol = dp83822_set_wol, \
.config_intr = dp83822_config_intr, \
.handle_interrupt = dp83822_handle_interrupt, \
.suspend = dp83822_suspend, \
.resume = dp83822_resume, \
}
#define DP8382X_PHY_DRIVER(_id, _name) \
{ \
PHY_ID_MATCH_MODEL(_id), \
.name = (_name), \
/* PHY_BASIC_FEATURES */ \
.soft_reset = dp83822_phy_reset, \
.config_init = dp8382x_config_init, \
.get_wol = dp83822_get_wol, \
.set_wol = dp83822_set_wol, \
.config_intr = dp83822_config_intr, \
.handle_interrupt = dp83822_handle_interrupt, \
.suspend = dp83822_suspend, \
.resume = dp83822_resume, \
}
static struct phy_driver dp83822_driver[] = {
DP83822_PHY_DRIVER(DP83822_PHY_ID, "TI DP83822"),
DP8382X_PHY_DRIVER(DP83825I_PHY_ID, "TI DP83825I"),
DP8382X_PHY_DRIVER(DP83826C_PHY_ID, "TI DP83826C"),
DP8382X_PHY_DRIVER(DP83826NC_PHY_ID, "TI DP83826NC"),
DP8382X_PHY_DRIVER(DP83825S_PHY_ID, "TI DP83825S"),
DP8382X_PHY_DRIVER(DP83825CM_PHY_ID, "TI DP83825M"),
DP8382X_PHY_DRIVER(DP83825CS_PHY_ID, "TI DP83825CS"),
};
module_phy_driver(dp83822_driver);
static struct mdio_device_id __maybe_unused dp83822_tbl[] = {
{ DP83822_PHY_ID, 0xfffffff0 },
{ DP83825I_PHY_ID, 0xfffffff0 },
{ DP83826C_PHY_ID, 0xfffffff0 },
{ DP83826NC_PHY_ID, 0xfffffff0 },
{ DP83825S_PHY_ID, 0xfffffff0 },
{ DP83825CM_PHY_ID, 0xfffffff0 },
{ DP83825CS_PHY_ID, 0xfffffff0 },
{ },
};
MODULE_DEVICE_TABLE(mdio, dp83822_tbl);
MODULE_DESCRIPTION("Texas Instruments DP83822 PHY driver");
MODULE_AUTHOR("Dan Murphy <dmurphy@ti.com");
MODULE_LICENSE("GPL v2");
--
Sincerely,
Hillman Lin
Hi Hillman,
When my customers use DP83822I, they have met some problems. The issue is very urgent and I need your great help.
The situation of customers is that ping can pass in the RMII mode, but the network speed can only be auto-negotiated at 10 Mbps and cannot be used at 100 Mbps.
The detailed issues are as follows:
root@:~# fec 2188000.ethernet eth0: Link is Down
root@:~# fec 2188000.ethernet eth0: Link is Up - 100Mbps/Full - flow control rx/tx
fec 2188000.ethernet eth0: Link is Down
fec 2188000.ethernet eth0: Link is Up - 100Mbps/Full - flow control rx/tx
fec 2188000.ethernet eth0: Link is Down
fec 2188000.ethernet eth0: Link is Up - 100Mbps/Full - flow control rx/tx
fec 2188000.ethernet eth0: Link is Down
fec 2188000.ethernet eth0: Link is Up - 100Mbps/Full - flow control rx/tx
fec 2188000.ethernet eth0: Link is Down
fec 2188000.ethernet eth0: Link is Up - 10Mbps/Full - flow control rx/tx
root@:~# ping 192.168.1.100
PING 192.168.1.100 (192.168.1.100) 56(84) bytes of data.
64 bytes from 192.168.1.100: icmp_seq=1 ttl=200 time=1.85 ms
64 bytes from 192.168.1.100: icmp_seq=2 ttl=200 time=0.909 ms
64 bytes from 192.168.1.100: icmp_seq=3 ttl=200 time=1.25 ms
64 bytes from 192.168.1.100: icmp_seq=4 ttl=200 time=1.01 ms
64 bytes from 192.168.1.100: icmp_seq=5 ttl=200 time=1.09 ms
64 bytes from 192.168.1.100: icmp_seq=6 ttl=200 time=1.04 ms
64 bytes from 192.168.1.100: icmp_seq=7 ttl=200 time=1.05 ms
64 bytes from 192.168.1.100: icmp_seq=8 ttl=200 time=1.22 ms
64 bytes from 192.168.1.100: icmp_seq=9 ttl=200 time=1.18 ms
64 bytes from 192.168.1.100: icmp_seq=10 ttl=200 time=1.24 ms
64 bytes from 192.168.1.100: icmp_seq=11 ttl=200 time=1.02 ms
64 bytes from 192.168.1.100: icmp_seq=12 ttl=200 time=0.970 ms
64 bytes from 192.168.1.100: icmp_seq=13 ttl=200 time=1.15 ms
64 bytes from 192.168.1.100: icmp_seq=14 ttl=200 time=1.02 ms
64 bytes from 192.168.1.100: icmp_seq=15 ttl=200 time=0.923 ms
64 bytes from 192.168.1.100: icmp_seq=16 ttl=200 time=1.17 ms
64 bytes from 192.168.1.100: icmp_seq=17 ttl=200 time=1.07 ms
64 bytes from 192.168.1.100: icmp_seq=18 ttl=200 time=1.08 ms
64 bytes from 192.168.1.100: icmp_seq=19 ttl=200 time=1.12 ms
64 bytes from 192.168.1.100: icmp_seq=21 ttl=200 time=1.10 ms
64 bytes from 192.168.1.100: icmp_seq=22 ttl=200 time=0.871 ms
64 bytes from 192.168.1.100: icmp_seq=24 ttl=200 time=1.18 ms
^C
--- 192.168.1.100 ping statistics ---
24 packets transmitted, 22 received, 8% packet loss, time 23042ms
rtt min/avg/max/mdev = 0.871/1.116/1.850/0.195 ms
root@:~#
phy addr value
0x0000 0x3100
0x0001 0x786d
0x0002 0x2000
0x0003 0xa240
0x0004 0x5e1
0x0005 0xcc61
0x0006 0xf
0x0007 0x2001
0x0008 0x4006
0x0009 0x0
0x000a 0x100
0x000b 0x1000
0x000f 0x0
0x0010 0x1817
0x0011 0x108
0x0012 0xf600
0x0013 0x2200
0x0016 0x100
0x0017 0xa1
0x0018 0x400
0x0019 0x3000
This issue is urgent and I look forward to your answers!
Hi Chen,
Thank you for sharing the register dump. I will discuss with the team on what other possible step we can perform on our side and get back to you as soon as possible. We will provide you an detail response by tomorrow.
Thank you for your patience
--
Regards,
Hillman Lin
Hi Chen,
May I ask what is customer's link partner? A block diagram on their setup would help.
When I read register 0x0005, it seems like the link partner does not support 100mbps through register 0x0005. Can you ask customer if they are able to see link with 100mbps with another DP83822 link partner?
--
Regards,
Hillman Lin