Part Number: DP83849IFVS-EVK
hello,
I'm not able to implement ethernet to fiber optic conversion in DP83849IFVS-EVKIT
i have connected ethernet cable to port A RJ45 [ AN0_A , AN1_A & ANEN_A are jumpered high]
both AN0 & AN1 lights were glowing and ANEN_A blinking when i send data
but still host is unreachable but i have tested the receiver side that device is working fine
Destination host unreachable is coming when i do ping test
could anyone tell me how can i test it and know that whether the data is transmitting or not
best regards,
Tex