Hello,
I have some questions about ESD441's leakage current.
- The data sheet has the leakage current specs (Typ and Max values) under the condition of VIO = 5.5 V, but are the Typ/Max specs available under different conditions of VIO = 0.1, 1, 2, and 3 V?
- What's the VIO condition of Figure 6-7 in the data sheet?
- What are the conditions when the leakage current goes up to the Max value of 50 nA?
- From the Figure 6-7, the ILEAK changes over temperatures are not so significant.
Best regards,
Shinichi Yokota