This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83TC812S-Q1: validation of sgmii failed

Part Number: DP83TC812S-Q1


Hello,

We have two DP83TC812SRHARQ1 PHYs each connected to a Microchip LAN9373 8-port switch on the SGMII port of the switch.

I'm attempting to bring up the PHYs under Linux and the following error occurs:

[ 9.925106] dp83812_read_straps: Strap is 0x20A
[ 10.146313] ksz-switch spi1.1 lan1 (uninitialized): validation of sgmii with support 00000000,00000000,00006280 and advertisement 00000000,00000000,00006280 failed: -EINVAL
[ 10.161820] ksz-switch spi1.1 lan1 (uninitialized): failed to connect to PHY: -EINVAL
[ 10.169684] ksz-switch spi1.1 lan1 (uninitialized): error -22 setting up PHY for tree 0, switch 1, port 3

The system is a iMX8QXP running Linux 6.1.1. 

I have downloaded the dp83tc812 driver from the following location: git.ti.com/gitweb
and enabled it in the kernel (CONFIG_DP83TC812_PHY=y).

Device tree of where the PHYs are defined:
&fec1 {
    pinctrl-names = "default";
    pinctrl-0 = <&pinctrl_fec1>;
    phy-mode = "rgmii";
    phy-handle = <&ethphy0>;
    fsl,magic-packet;
    status = "okay";
    phy-supply = <&reg_phy0_pwr>;
    phy-reset-gpios = <&lsio_gpio1 2 GPIO_ACTIVE_LOW>;
    phy-reset-on-resume;
    phy-reset-duration = <100>;
    phy-reset-post-delay = <100>;

    mdio {
        #address-cells = <1>;
        #size-cells = <0>;

        lan0phy: ethernet-phy@15 {
            compatible = "ethernet-phy-ieee802.3-c22";
            reg = <15>;
            reset-gpios = <&lsio_gpio3 17 GPIO_ACTIVE_LOW>;
        };

        lan1phy: ethernet-phy@12 { 
            compatible = "ethernet-phy-ieee802.3-c22";
            reg = <12>;
            reset-gpios = <&lsio_gpio3 23 GPIO_ACTIVE_LOW>;
        };

        // other phys not shown...
    };
};



Device tree of where the DSA switch ports are defined:
switch0: switch@0 {
    compatible 		   	= "microchip,lan9373";
    reg 		       	= <0>;
    spi-max-frequency  	= <12000000>;
    dsa,member			= <0 0>;
    status 			   	= "okay";

    ports {
        port@3 { 
            reg = <3>;
            phy-mode = "sgmii";
            phy-handle = <&lan0phy>;
            label = "lan0";
        };

        // other ports not shown...
    };
};

switch1: switch@1 {
    compatible 		   	= "microchip,lan9373";
    reg 		       	= <1>;
    spi-max-frequency  	= <12000000>;
    dsa,member			= <0 1>;
    status 			   	= "okay";
    
    ports {
        port@3 {
            reg = <3>;
            phy-mode = "sgmii";
            phy-handle = <&lan1phy>;
            label = "lan1";
        };

        // other ports not shown...
    };
};
The driver is successful in querying the straps  (dp83812_read_straps: Strap is 0x20A) but unable to proceed past the "validation of sgmii with support 00000000,00000000,00006280 and advertisement 00000000,00000000,00006280 failed: -EINVAL" error.

Is there any adivce on how to solve this error?

Thanks,
Simon
  • Hello,

    Is the driver dp83tc812.c at the following location the latest version of the driver for DP83TC812S-Q1?

    https://git.ti.com/gitweb?p=ti-analog-linux-kernel/analog-linux.git;a=blob;f=drivers/net/phy/dp83tc812.c;h=0c594375f188d40299603628a0636947cfea35bf;hb=f973f3deb81b1f44aa4c33b275a342e28fc982fd

    I found that it had a NULL pointer dereference within the dp83812_read_straps() called during dp83812_probe(). The below patch was required to fix it:

    @@ -486,6 +486,8 @@ static int dp83812_probe(struct phy_device *phydev)
            dp83812 = devm_kzalloc(&phydev->mdio.dev, sizeof(*dp83812), GFP_KERNEL);
            if (!dp83812)
                    return -ENOMEM;
    +       
    +       phydev->priv = dp83812;
     
            ret = dp83812_read_straps(phydev);
            if (ret)
    

    Thanks

    Simon

  • Hello Simon,

    Can you please verify with the driver attached?

    // SPDX-License-Identifier: GPL-2.0
    /*
     * Driver for the Texas Instruments DP83TC812 PHY
     *
     * Copyright (C) 2021 Texas Instruments Incorporated - http://www.ti.com/
     *
     */
    
    #include <linux/ethtool.h>
    #include <linux/etherdevice.h>
    #include <linux/kernel.h>
    #include <linux/mii.h>
    #include <linux/module.h>
    #include <linux/of.h>
    #include <linux/phy.h>
    #include <linux/netdevice.h>
    
    #define DP83TC812_CS1_0_PHY_ID	0x2000a270
    #define DP83TC812_CS2_0_PHY_ID	0x2000a271
    #define DP83TC813_CS2_0_PHY_ID	0x2000a211
    #define DP83TC814_CS2_0_PHY_ID	0x2000a261
    
    #define DP83812_DEVADDR		0x1f
    #define DP83812_DEVADDR_MMD1	0x1
    
    #define DP83812_STRAP		0x45d
    #define MII_DP83812_SGMII_CTRL	0x608
    #define SGMII_CONFIG_VAL	0x027B
    #define MII_DP83812_RGMII_CTRL	0x600
    #define MII_DP83812_INT_STAT1	0x12
    #define MII_DP83812_INT_STAT2	0x13
    #define MII_DP83812_INT_STAT3	0x18
    #define MII_DP83812_RESET_CTRL	0x1f
    
    #define DP83812_HW_RESET	BIT(15)
    #define DP83812_SW_RESET	BIT(14)
    
    /* INT_STAT1 bits */
    #define DP83812_RX_ERR_CNT_HALF_FULL_INT_EN	BIT(0)
    #define DP83812_TX_ERR_CNT_HALF_FULL_INT_EN	BIT(1)
    #define DP83812_MS_TRAIN_DONE_INT_EN		BIT(2)
    #define DP83812_ESD_EVENT_INT_EN		BIT(3)
    #define DP83812_LINK_STAT_INT_EN		BIT(5)
    #define DP83812_ENERGY_DET_INT_EN		BIT(6)
    #define DP83812_LINK_QUAL_INT_EN		BIT(7)
    
    /* INT_STAT2 bits */
    #define DP83812_JABBER_INT_EN		BIT(0)
    #define DP83812_POL_INT_EN		BIT(1)
    #define DP83812_SLEEP_MODE_INT_EN	BIT(2)
    #define DP83812_OVERTEMP_INT_EN		BIT(3)
    #define DP83812_FIFO_INT_EN		BIT(4)
    #define DP83812_PAGE_RXD_INT_EN		BIT(5)
    #define DP83812_OVERVOLTAGE_INT_EN	BIT(6)
    #define DP83812_UNDERVOLTAGE_INT_EN	BIT(7)
    
    /* INT_STAT3 bits */
    #define DP83812_LPS_INT_EN		BIT(0)
    #define DP83812_WUP_INT_EN		BIT(1)
    #define DP83812_WAKE_REQ_INT_EN		BIT(2)
    #define DP83811_NO_FRAME_INT_EN		BIT(3)
    #define DP83811_POR_DONE_INT_EN		BIT(4)
    #define DP83812_SLEEP_FAIL_INT_EN	BIT(5)
    
    /* RGMII_CTRL bits */
    #define DP83812_RGMII_EN		BIT(3)
    
    /* SGMII CTRL bits */
    #define DP83812_SGMII_AUTO_NEG_EN	BIT(0)
    #define DP83812_SGMII_EN		BIT(9)
    
    /* Strap bits */
    #define DP83812_MASTER_MODE	BIT(9)
    #define DP83812_RGMII_IS_EN	BIT(7)
    
    /* RGMII ID CTRL */
    #define DP83812_RGMII_ID_CTRL	0x602
    #define DP83812_RX_CLK_SHIFT	BIT(1)
    #define DP83812_TX_CLK_SHIFT	BIT(0)
    
    enum dp83812_chip_type {
    	DP83812_CS1 = 0,
    	DP83812_CS2,
    	DP83813_CS2,
    	DP83814_CS2,
    };
    
    struct dp83812_init_reg {
    	int	reg;
    	int	val;
    };
    
    static const struct dp83812_init_reg dp83812_master_cs1_0_init[] = {
    	{0x523, 0x0001},
    	{0x800, 0xf864},
    	{0x803, 0x1552},
    	{0x804, 0x1a66},
    	{0x805, 0x1f7b},
    	{0x81f, 0x2a88},
    	{0x825, 0x40e5},
    	{0x82b, 0x7f3f},
    	{0x830, 0x0543},
    	{0x836, 0x5008},
    	{0x83a, 0x08e0},
    	{0x83b, 0x0845},
    	{0x83e, 0x0445},
    	{0x855, 0x9b9a},
    	{0x85f, 0x2010},
    	{0x860, 0x6040},
    	{0x86c, 0x1333},
    	{0x86b, 0x3e10},
    	{0x872, 0x88c0},
    	{0x873, 0x0003},
    	{0x879, 0x000f},
    	{0x87b, 0x0070},
    	{0x87c, 0x003f},
    	{0x89e, 0x00aa},
    	{0x523, 0x0000},
    };
    
    static const struct dp83812_init_reg dp83812_master_cs2_0_init[] = {
    	{0x523, 0x0001},
    	{0x81C, 0x0fe2},
    	{0x872, 0x0300},
    	{0x879, 0x0f00},
    	{0x806, 0x2952},
    	{0x807, 0x3361},
    	{0x808, 0x3D7B},
    	{0x83E, 0x045F},
    	{0x834, 0x8000},
    	{0x862, 0x00E8},
    	{0x896, 0x32CB},
    	{0x03E, 0x0009},
    	{0x01f, 0x4000},
    	{0x523, 0x0000},
    };
    
    static const struct dp83812_init_reg dp83812_slave_cs1_0_init[] = {
    	{0x523, 0x0001},
    	{0x803, 0x1b52},
    	{0x804, 0x216c},
    	{0x805, 0x277b},
    	{0x827, 0x3000},
    	{0x830, 0x0543},
    	{0x83a, 0x0020},
    	{0x83c, 0x0001},
    	{0x855, 0x9b9a},
    	{0x85f, 0x2010},
    	{0x860, 0x6040},
    	{0x86c, 0x0333},
    	{0x872, 0x88c0},
    	{0x873, 0x0021},
    	{0x879, 0x000f},
    	{0x87b, 0x0070},
    	{0x87c, 0x0002},
    	{0x897, 0x003f},
    	{0x89e, 0x00a2},
    	{0x510, 0x000f},
    	{0x523, 0x0000},
    };
    
    static const struct dp83812_init_reg dp83812_slave_cs2_0_init[] = {
    	{0x523, 0x0001},
    	{0x873, 0x0821},
    	{0x896, 0x22ff},
    	{0x89E, 0x0000},
    	{0x01f, 0x4000},
    	{0x523, 0x0000},
    };
    
    struct dp83812_private {
    	int chip;
    	bool is_master;
    	bool is_rgmii;
    	bool is_sgmii;
    };
    
    static int dp83812_read_straps(struct phy_device *phydev)
    {
    	struct dp83812_private *dp83812 = phydev->priv;
    	int strap;
    
    	strap = phy_read_mmd(phydev, DP83812_DEVADDR, DP83812_STRAP);
    	if (strap < 0)
    		return strap;
    
    	printk("%s: Strap is 0x%X\n", __func__, strap);
    	if (strap & DP83812_MASTER_MODE)
    		dp83812->is_master = true;
    
    	if (strap & DP83812_RGMII_IS_EN)
    		dp83812->is_rgmii = true;
    	return 0;
    };
    
    static int dp83812_reset(struct phy_device *phydev, bool hw_reset)
    {
    	int ret;
    
    	if (hw_reset)
    		ret = phy_write_mmd(phydev, DP83812_DEVADDR, MII_DP83812_RESET_CTRL,
    				DP83812_HW_RESET);
    	else
    		ret = phy_write_mmd(phydev, DP83812_DEVADDR, MII_DP83812_RESET_CTRL,
    				DP83812_SW_RESET);
    
    	if (ret)
    		return ret;
    
    	mdelay(100);
    
    	return 0;
    }
    
    static int dp83812_phy_reset(struct phy_device *phydev)
    {
    	int err;
    	int ret;
    
    	err = phy_write_mmd(phydev, DP83812_DEVADDR, MII_DP83812_RESET_CTRL, DP83812_HW_RESET);
    	if (err < 0)
    		return err;
    
    	ret = dp83812_read_straps(phydev);
    	if (ret)
    		return ret;
    
    	return 0;
    }
    
    static int dp83812_write_seq(struct phy_device *phydev, const struct
    				dp83812_init_reg *init_data, int size)
    {
    	int ret;
    	int i;
    
    	for (i = 0; i < size; i++) {
    		ret = phy_write_mmd(phydev, DP83812_DEVADDR, init_data[i].reg,
    					init_data[i].val);
    	if (ret)
    		return ret;
    	}
    	return 0;
    }
    
    static int dp83812_chip_init(struct phy_device *phydev)
    {
    	struct dp83812_private *dp83812 = phydev->priv;
    	int ret;
    
    	ret = dp83812_reset(phydev, true);
    	if (ret)
    		return ret;
    
    	phydev->autoneg = AUTONEG_DISABLE;
    	phydev->speed = SPEED_100;
    	phydev->duplex = DUPLEX_FULL;
    	linkmode_set_bit(ETHTOOL_LINK_MODE_100baseT_Full_BIT,
    		 phydev->supported);
    
    	if (dp83812->is_master)
    		ret = phy_write_mmd(phydev, DP83812_DEVADDR_MMD1, 0x0834, 0xc001);
    		// ret = phy_write_mmd(phydev, DP83812_DEVADDR, 0x0834, 0xc001);
    	else
    		ret = phy_write_mmd(phydev, DP83812_DEVADDR_MMD1, 0x0834, 0x8001);
    		// ret = phy_write_mmd(phydev, DP83812_DEVADDR, 0x0834, 0x8001);
    
    	switch (dp83812->chip) {
    	case DP83812_CS1:
    		if (dp83812->is_master)
    			ret = dp83812_write_seq(phydev,
    						dp83812_master_cs1_0_init,
    						ARRAY_SIZE(dp83812_master_cs1_0_init));
    		else
    			ret = dp83812_write_seq(phydev,
    						dp83812_slave_cs1_0_init,
    						ARRAY_SIZE(dp83812_slave_cs1_0_init));
    	break;
    	case DP83812_CS2:
    		if (dp83812->is_master)
    			ret = dp83812_write_seq(phydev,
    						dp83812_master_cs2_0_init,
    						ARRAY_SIZE(dp83812_master_cs2_0_init));
    		else
    			ret = dp83812_write_seq(phydev,
    						dp83812_slave_cs2_0_init,
    						ARRAY_SIZE(dp83812_slave_cs2_0_init));
    	break;
    	case DP83813_CS2:
    		if (dp83812->is_master)
    			ret = dp83812_write_seq(phydev,
    						dp83812_master_cs2_0_init,
    						ARRAY_SIZE(dp83812_master_cs2_0_init));
    		else
    			ret = dp83812_write_seq(phydev,
    						dp83812_slave_cs2_0_init,
    						ARRAY_SIZE(dp83812_slave_cs2_0_init));
    	break;
    	case DP83814_CS2:
    		if (dp83812->is_master)
    			ret = dp83812_write_seq(phydev,
    						dp83812_master_cs2_0_init,
    						ARRAY_SIZE(dp83812_master_cs2_0_init));
    		else
    			ret = dp83812_write_seq(phydev,
    						dp83812_slave_cs2_0_init,
    						ARRAY_SIZE(dp83812_slave_cs2_0_init));
    	break;
    	default:
    		return -EINVAL;
    	};
    
    	if (ret)
    		return ret;
    
    	mdelay(10);
    	// phy_write_mmd(phydev, DP83812_DEVADDR, 0x523, 0x00);
    	/* Do a soft reset to restart the PHY with updated values */
    	return dp83812_reset(phydev, false);
    }
    
    static int dp83812_config_init(struct phy_device *phydev)
    {
    	struct device *dev = &phydev->mdio.dev;
    	s32 rx_int_delay;
    	s32 tx_int_delay;
    	int rgmii_delay;
    	int value, ret;
    
    	ret = dp83812_chip_init(phydev);
    	if (ret)
    		return ret;
    
    	if (phy_interface_is_rgmii(phydev)) {
    		rx_int_delay = phy_get_internal_delay(phydev, dev, NULL, 0,
    						      true);
    
    		if (rx_int_delay <= 0)
    			rgmii_delay = 0;
    		else
    			rgmii_delay = DP83812_RX_CLK_SHIFT;
    
    		tx_int_delay = phy_get_internal_delay(phydev, dev, NULL, 0,
    						      false);
    		if (tx_int_delay <= 0)
    			rgmii_delay &= ~DP83812_TX_CLK_SHIFT;
    		else
    			rgmii_delay |= DP83812_TX_CLK_SHIFT;
    
    		if (rgmii_delay) {
    			ret = phy_set_bits_mmd(phydev, DP83812_DEVADDR_MMD1,
    					       DP83812_RGMII_ID_CTRL,
    					       rgmii_delay);
    			if (ret)
    				return ret;
    		}
    	}
    
    	if (phydev->interface == PHY_INTERFACE_MODE_SGMII) {
    		value = phy_read(phydev, MII_DP83812_SGMII_CTRL);
    		ret = phy_write_mmd(phydev, DP83812_DEVADDR, MII_DP83812_SGMII_CTRL,
    				SGMII_CONFIG_VAL);
    	if (ret < 0)
    		return ret;
    	}
    
    	return 0;
    }
    
    static int dp83812_ack_interrupt(struct phy_device *phydev)
    {
    	int err;
    
    	err = phy_read(phydev, MII_DP83812_INT_STAT1);
    	if (err < 0)
    		return err;
    
    	err = phy_read(phydev, MII_DP83812_INT_STAT2);
    	if (err < 0)
    		return err;
    
    	err = phy_read(phydev, MII_DP83812_INT_STAT3);
    	if (err < 0)
    		return err;
    
    	return 0;
    }
    
    static int dp83812_config_intr(struct phy_device *phydev)
    {
    	int misr_status, err;
    
    	if (phydev->interrupts == PHY_INTERRUPT_ENABLED) {
    		misr_status = phy_read(phydev, MII_DP83812_INT_STAT1);
    		if (misr_status < 0)
    			return misr_status;
    
    		misr_status |= (DP83812_ESD_EVENT_INT_EN |
    				DP83812_LINK_STAT_INT_EN |
    				DP83812_ENERGY_DET_INT_EN |
    				DP83812_LINK_QUAL_INT_EN);
    
    		err = phy_write(phydev, MII_DP83812_INT_STAT1, misr_status);
    		if (err < 0)
    			return err;
    
    		misr_status = phy_read(phydev, MII_DP83812_INT_STAT2);
    		if (misr_status < 0)
    			return misr_status;
    
    		misr_status |= (DP83812_SLEEP_MODE_INT_EN |
    				DP83812_OVERTEMP_INT_EN |
    				DP83812_OVERVOLTAGE_INT_EN |
    				DP83812_UNDERVOLTAGE_INT_EN);
    
    		err = phy_write(phydev, MII_DP83812_INT_STAT2, misr_status);
    		if (err < 0)
    			return err;
    
    		misr_status = phy_read(phydev, MII_DP83812_INT_STAT3);
    		if (misr_status < 0)
    			return misr_status;
    
    		misr_status |= (DP83812_LPS_INT_EN |
    				DP83812_WAKE_REQ_INT_EN |
    				DP83811_NO_FRAME_INT_EN |
    				DP83811_POR_DONE_INT_EN);
    
    		err = phy_write(phydev, MII_DP83812_INT_STAT3, misr_status);
    
    	} else {
    		err = phy_write(phydev, MII_DP83812_INT_STAT1, 0);
    		if (err < 0)
    			return err;
    
    		err = phy_write(phydev, MII_DP83812_INT_STAT2, 0);
    		if (err < 0)
    			return err;
    
    		err = phy_write(phydev, MII_DP83812_INT_STAT3, 0);
    	}
    
    	return err;
    }
    
    #if 0
    static irqreturn_t dp83812_handle_interrupt(struct phy_device *phydev)
    {
    	bool trigger_machine = false;
    	int irq_status;
    
    	/* The INT_STAT registers 1, 2 and 3 are holding the interrupt status
    	 * in the upper half (15:8), while the lower half (7:0) is used for
    	 * controlling the interrupt enable state of those individual interrupt
    	 * sources. To determine the possible interrupt sources, just read the
    	 * INT_STAT* register and use it directly to know which interrupts have
    	 * been enabled previously or not.
    	 */
    	irq_status = phy_read(phydev, MII_DP83812_INT_STAT1);
    	if (irq_status < 0) {
    		phy_error(phydev);
    		return IRQ_NONE;
    	}
    	if (irq_status & ((irq_status & GENMASK(7, 0)) << 8))
    		trigger_machine = true;
    
    	irq_status = phy_read(phydev, MII_DP83812_INT_STAT2);
    	if (irq_status < 0) {
    		phy_error(phydev);
    		return IRQ_NONE;
    	}
    	if (irq_status & ((irq_status & GENMASK(7, 0)) << 8))
    		trigger_machine = true;
    
    	irq_status = phy_read(phydev, MII_DP83812_INT_STAT3);
    	if (irq_status < 0) {
    		phy_error(phydev);
    		return IRQ_NONE;
    	}
    	if (irq_status & ((irq_status & GENMASK(7, 0)) << 8))
    		trigger_machine = true;
    
    	if (!trigger_machine)
    		return IRQ_NONE;
    
    	phy_trigger_machine(phydev);
    
    	return IRQ_HANDLED;
    }
    #endif
    
    static int dp83812_config_aneg(struct phy_device *phydev)
    {
    	int value, ret;
    
    	if (phydev->interface == PHY_INTERFACE_MODE_SGMII) {
    		value = phy_read(phydev, MII_DP83812_SGMII_CTRL);
    		ret = phy_write_mmd(phydev, DP83812_DEVADDR, MII_DP83812_SGMII_CTRL,
    				SGMII_CONFIG_VAL);
    		if (ret < 0)
    			return ret;
    	}
    	
    	return genphy_config_aneg(phydev);
    }
    
    
    
    static int dp83812_probe(struct phy_device *phydev)
    {
    	struct dp83812_private *dp83812;
    	int ret;
    
    	dp83812 = devm_kzalloc(&phydev->mdio.dev, sizeof(*dp83812), GFP_KERNEL);
    	if (!dp83812)
    		return -ENOMEM;
    
    	phydev->priv = dp83812;					
    	ret = dp83812_read_straps(phydev);
    	if (ret)
    		return ret;
    
    	switch (phydev->phy_id) {
    	case DP83TC812_CS1_0_PHY_ID:
    		dp83812->chip = DP83812_CS1;
    	break;
    	case DP83TC812_CS2_0_PHY_ID:
    		dp83812->chip = DP83812_CS2;
    	break;
    	case DP83TC813_CS2_0_PHY_ID:
    		dp83812->chip = DP83813_CS2;
    		break;
    	case DP83TC814_CS2_0_PHY_ID:
    		dp83812->chip = DP83814_CS2;
    	break;
    	default:
    	return -EINVAL;
    	};
    /* vikram : above code added to switch between different phy ids */
    
    	return dp83812_config_init(phydev);
    }
    
    #define DP83812_PHY_DRIVER(_id, _name)				\
    	{							\
    		PHY_ID_MATCH_EXACT(_id),			\
    		.name           = (_name),			\
    		.probe          = dp83812_probe,		\
    		/* PHY_BASIC_FEATURES */			\
    		.soft_reset     = dp83812_phy_reset,		\
    		.config_init    = dp83812_config_init,		\
    		.config_aneg = dp83812_config_aneg,		\
    		.ack_interrupt = dp83812_ack_interrupt,		\
    /*if 0								\
    		.handle_interrupt = dp83812_handle_interrupt,	\
    #endif	*/							\
    		.config_intr = dp83812_config_intr,		\
    		.suspend = genphy_suspend,			\
    		.resume = genphy_resume,			\
    	}
    
    static struct phy_driver dp83812_driver[] = {
    	DP83812_PHY_DRIVER(DP83TC812_CS1_0_PHY_ID, "TI DP83TC812CS1.0"),
    	DP83812_PHY_DRIVER(DP83TC812_CS2_0_PHY_ID, "TI DP83TC812CS2.0"),
    	DP83812_PHY_DRIVER(DP83TC813_CS2_0_PHY_ID, "TI DP83TC813CS2.0"),
    	DP83812_PHY_DRIVER(DP83TC814_CS2_0_PHY_ID, "TI DP83TC814CS2.0"),
    	};
    
    module_phy_driver(dp83812_driver);
    
    static struct mdio_device_id __maybe_unused dp83812_tbl[] = {
    	{ PHY_ID_MATCH_EXACT(DP83TC812_CS1_0_PHY_ID) },
    	{ PHY_ID_MATCH_EXACT(DP83TC812_CS2_0_PHY_ID) },
    	{ PHY_ID_MATCH_EXACT(DP83TC813_CS2_0_PHY_ID) },
    	{ PHY_ID_MATCH_EXACT(DP83TC814_CS2_0_PHY_ID) },
    	{ },
    };
    MODULE_DEVICE_TABLE(mdio, dp83812_tbl);									   
    
    MODULE_DESCRIPTION("Texas Instruments DP83TC812 PHY driver");
    MODULE_AUTHOR("Hari Nagalla <hnagalla@ti.com");
    MODULE_LICENSE("GPL");
    

    --
    Regards,
    Gokul.

  • Hi Gokul,

    Thanks for providing the updated driver. Confirming that the updated driver solved my issue.

    Regards,

    Simon