Part Number: AM26C32
Hi,
I need to make a universal Differential receiver module.
The specification is that I am using CAT5 and I have 4 rows of SPI LED 800khz max throughput Each row separated by 1m.
When I am sending from the LED SPI controller I get interference greater than 10m . In some cased I need to go up to 30m
So in searching the web , I noticed that some companies used differential drivers. I purchased a whole lot of the AM26C32CN (25 pcs) and AM26C31CN(5) .
the idea is to make one design for the receivers so that I can produce in volume the same item and use it for the 4 outputs. Each output is 1m apart.
The module design I thought would have the opportunity for all 4 outputs of the receiver which is battery powered by 2 x 3.7v Batteries and using a 5 volt regulator
Then the 4th module in the chain would have the termination resistors avail on a dip switch as the requirement of being the last Receiver in the chain being terminated.
Each module will have Ethernet in and bridged to Ethernet out with a tap to the receiver chip.
Before I manufacture the samples of this item and design the board with the strict rules for the differential lines as per the datasheet. I wanted to make sure this circuit was ok of should there be any other design changes. I do not know what the Value of G and (NOT G) should be . I suspect the G should be +5v and (Not G) not connected.
Any assistance and guidance on this design would be greatly appreciated.
I manufacture LED Dancefloors in South Africa which this is what I require to make the floors run correctly without corruption on distances further than 10m
Thank youUniversal Differential Receiver Circuit.pdf