This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Can DP83826I VDDIO run at 2.5V?

Part Number: DP83826I

Will DP83826I operate with VDDIO of 2.5V?

We need to interface this to 2.5V logic, and don't want to use a level shifter if we can avoid it.  Inputs to the DP83826I are ok, but at 3.3V VDDIO the DP82826I can overdrive the MAC 2.5V inputs.

Datasheet specifies device at 1.8V and 3.3V. 

"Automatic supply configuration within the DP83826 allows for any combination of VDDIO supply without the need for additional configuration settings." from datasheet section 9.1.