Part Number: DP83TG720S-Q1
Hi,
I am working with Automotive ethernet DP83TG720SWRHATQ1. I have received the driver source code. I added the same to my BSP. I have also enabled CONFIG_DP83TG720_PHY in make menuconfig. the driver source get compiled and after i flash, It does not probe. Do i need to do any further changes.
Below is my device tree configuration.
&eqos {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_eqos>;
phy-mode = "rgmii-id";
phy-handle = <ðphy0>;
fsl,magic-packet;
nvmem-cells = <&fec_mac1>;
nvmem-cell-names = "mac-address";
snps,reset-gpios = <&lsio_gpio0 20 GPIO_ACTIVE_LOW>;
snps,reset-delays-us = <10 20 200000>;
status = "okay";
mdio {
compatible = "snps,dwmac-mdio";
#address-cells = <1>;
#size-cells = <0>;
ethphy0: ethernet-phy@0 {
compatible = "ethernet-phy-ieee802.3-c22";
reg = <0>;
status = "okay";
};
};
};
Regards,
Akhil K