Part Number: SN65LVDS31-EP
Is it necessary to have an output series resistor on the LVDS outputs when driving a 100ohm differential load?
Output load is shown to be 5 ohms so a 45-ohm series resistor should help with reflections?
- Michael
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN65LVDS31-EP
Is it necessary to have an output series resistor on the LVDS outputs when driving a 100ohm differential load?
Output load is shown to be 5 ohms so a 45-ohm series resistor should help with reflections?
- Michael
Hello Michael,
It's not necessary to add series resistors on the output of the LVDS driver. The output characteristic impedance should match the differential load. In other words, if using a 100 Ω load, then each output trace should be 50 Ω. See image below.

Regards,
Josh