This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCAN1043A-Q1: Does TCAN1043A-Q1 Covered SAE J2284-3, if does not, which part can not cover?

Part Number: TCAN1043A-Q1

Does TCAN1043A-Q1 Covered SAE J2284-3,

if does not, which part can not be covered?

  • Hi Song-hwan,

    SAE J2284-3 is a node-level specification that applies to the ECU as a whole. The specification references the ISO 11898-2 CAN physical layer standard as its electrical requirements for the CAN portion of the system, so any transceiver that supports this specification (including TCAN1043A) can be used for a SAE J2284-3 compliant system design. 

    Let me know if you have any more questions. 

    Regards, 
    Eric Schott 

  • Thank you for your kind & detail answer, that is really helpful!!