Part Number: TCA9543A
Can it still work normally when VDPUx<VCC*0.7(VIH)?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Clemens,
Can it be understood that VDPUm cannot be lower than VCC*0.7 and VDPU0/1 is not limited by VCC?
Thank you!
VDPUM must be higher than 70% of VCC to allow the master to control the channels. All VDPUM and VDPUx are limited by the maximum pass-through voltage of the pass-gate transistors (see section 9.2.1 and figure 17).
Hi Jian,
The figure that Clemens is referencing is the pass gate voltage spec vs. VCC graph.

Vpass is defined as the smallest pull-up voltage (VDPUM or VDPUx) in the system. Based off this pull-up voltage, the user can determine what is the highest VCC can be used in the system to ensure correct voltage translation.
Also from the recommended operating specs.
1.65V < VCC < 5.5V
1.65V < VDPUx < 5.5V
1.65V < VDPUM < 5.5V
Regards,
Tyler