Part Number: TCAN4550
Hi Expert,
In customer's design, the GPO1, GPO2 of TCAN4550 is not connected.
The engineer is asking the impact of watchdog function?
Thanks
Eric
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Eric,
If they want to use the watchdog function, there are two ways of setting the trigger bit. The GPIO1 pin can be configured to reset the timer on a rising or falling edge. The other option is a SPI write to 0x0800[18].
If the GPIO1 pin is not connected, and they want to use the watchdog function, they will have to use the SPI option for resetting the timer.
Regards,
Jonathan