Part Number: DS160PT801
Hi,
In the datasheet of DS160PT801, the retimer application is specified by placing the same in motherboard and riser card.
Can it be placed in a add in card?
Thanks and Regards,
Shekha Shoukath
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS160PT801
Hi,
In the datasheet of DS160PT801, the retimer application is specified by placing the same in motherboard and riser card.
Can it be placed in a add in card?
Thanks and Regards,
Shekha Shoukath
Greetings,
PCIe is point to point. Therefor there are not multiple end points. Clock is used by the retimer and it is buffered for the single end point.
Regards, Nasser
Hi,
If we need 4x4 output connector instead od x16 connector, then don't we need a clock buffer to provide 4 RefClk out to four port?
Regards,
Shekha Shoukath
Greetings,
Yes you would need one 100MHz clock signal. Please refer to the PCIe specifications. This clock is part of the PCIe connector no matter whether you use X4 or others such as X16 lanes.
Regards, Nasser