Part Number: DS90UB948-Q1
Other Parts Discussed in Thread: DS90UB949A-Q1, DS90CF386, DS90CF388A
Hello,
Starting with the SerDes-pair 'DS90UB949A-Q1 to DS90UB948-Q1', I have understood that I need to use the full (dual channel) OpenLDI-interface from DS90UB948 (6 data-pairs and 2 clock-pairs) to get 1920x1200@60Hz.
I have only found a way to create TMDS from OpenLDI by using DS90CF386 and then ADV7511. But the problem is that DS90CF386 only have one channel OpenLDI input interface which limits my output frequency to 96MHz pixel clock. And by my calculations I will need to be north of 152MHz.
Is there another LVDS-to-Parallel converter that can handle dual channel OpenLDI? Maybe also a TMDS-converter that can handle whatever IC you suggest? I am open to suggestions.
Cheers