Part Number: DS90UB941AS-Q1
Hi TI experts,
I found there are different descriptions on the "CLOCK Mode" in the MODE_SEL1 configuration.
In table 8-8, it shows that the FPDlink will be generated from REFCLK pin when CLOCK Mode = 0 and generated from DSI when CLOCK mode =1.

However, in Table 8-11 and 8.4.2.1 DSI Clock Modes section, it describes that this bit only configure the DSI clock mode - continuous or discontinuous.


Which descriptions is correct?
In my test, the FPDlink is still generated from DSI clock when MODE_SEL1 is changed from MODE1 to MODE 5.
If I want to use an external reference clock from the REFCLK pin, do I only need to change BRIDGE_CFG[1:0] to 01 without changing the MODE_SEL1 configuration?
Thanks.