Part Number: SN75C3232
Other Parts Discussed in Thread: MAX3232, TRSF3232, TRSF3232E,
Hi team,
The customer has previously used MAX3232CDWΩ (MAX3232 3V to 5.5V Multichannel RS-232 Line Driver/Receiver)
MAX3232CDW => runs at speeds of up to 250 kbit/s.
Considering that UART currently requires higher speeds (921600), they want to replace the new IC with the original PCB.
We find TI corresponding solution is
SN65C3232DW
Or
SN75C3232DW
May I know the difference of 65 / 75?
Is there any other recommend solution?
Thanks!
BRs,
Jamie