This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83822I: Phy address configuration issue cannot set 0x0000

Part Number: DP83822I

Hi

One of my customer is facing the issue in configurating the Ethernet PHY address. 

The PHY address is set to 00000 by the below configuration:

 

Signal name 

MODE 

External PU/PD resistor 

COL 

1 

External 2.2 Kohm  

RX_D0 

1 

No external PD (Internal PD resistor) 

RX_D1 

1 

No external PD (Internal PD resistor) 

RX_D2 

1 

No external PD (Internal PD resistor) 

RX_D3 

2 

External 10K (PU) and 2.49k (PD) 

 

they have made the configuration as above but still the PHY doesn't take this address and seems to be stuck on 0x01 which is the default address of the PHY.

operating DP83822 in RGMII mode and have made the configuration as below:

 

Signal name 

MODE 

External PU/PD resistor 

RX_ER 

3 

6.2 K(PU) and 1.96k(PD) 

 

I asked to verify the bootstrap resistors configuration as per data sheet as 1.96k but still the issue persists. 

The voltage levels they see at these pins are as mentioned below:

  1. RX_D0 : 0.011 V
  2. RX_D1: 0.233 V
  3. RX_D2: 0.202 V
  4. RX_D3: 0.231 V
  5. COL: 0.011 V

out of two PHYs they connect, they could not verify the individual addresses and cannot point to the individual one.