Part Number: SN65DPHY440SS
Hello team,
This is related question to the previous thread below.
https://e2e.ti.com/support/interface-group/interface/f/interface-forum/1275393/sn65dphy440ss-double-cable-length-if-use-2-devices-in-series
2 repeater doesnt achieve exact double cable length extension, why is this?
If this device is like a buffer, the signal of 1s and 0s will be regenerated at the device with internal comparator, so if 100 repeaters are used, it should be able to extend 100 times. Isn't it right?
Also is it possible to estimate the effectiveness when using 2 of this repeater device. I know PCB and cable loss will be there, but is there any rule of thumb?
Best Regards,
Kei Kuwahara