Part Number: DS90CR486
Other Parts Discussed in Thread: DS90UB948-Q1
Hi,
Is the DS90CR486 compatible with the deserializer DS90UB948-Q1? The Deserializer outputs single OLDI up to 133MHz, but the DS90CR486 has 7 data channels for input with a single CLK channel. Do I need all 7 inputs for 133 MHz CLK? Or can I connect the single OLDI interface directly to 4 input channels of the DS90CR486, leaving 3 channels NC?