Part Number: THVD4431
Hi,
The maximum short circuit current in RS485 mode is mentioned as 250mA.
Is there any over-current protection in the chip so that the it can cut off below the short circuit current or should the power supply be rated to handle this current.
If we implement an external over current protection, can we set it at 100mA such that it does not affect the normal operation?