Part Number: TCAN4550
Please help check if this schematic is correct
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I have reviewed the schematic and I have the following comments:
- I don't know if the VIO voltage is 3.3V or 5V by the power net name of "VIO18_PMU" and whether this name implies that the voltage level is 1.8V. The TCAN4550 only supports 3.3V or 5V voltage levels. If 1.8V support is needed, the TCAN4551 should be considered, but this device does not support a crystal when VIO = 1.8V.
- The crystal oscillator circuit has all the components needed to optimize the performance, in particular the series resistor between OSC1 and the crystal. The cap and resistor values may need to be adjusted for optimal performance as outlined in the TCAN455x Clock Optimization and Design Guidelines application Note. (Link)
- The nINT and GPO2 pins have an open-drain architecture and require a pull up resistor to the VIO voltage.
- Just a Note that the RST (reset) pin is active High, so it will need to be held low during normal operation
Let me know if there are any additional questions.
Regards,
Jonathan