hello
Could you explain the possible reason of link up 0x01=0x0065 with SQI reg871=0?
1. Constant reading for tens of times with stable reading when ethernet communication doesn't work well
2. After 30min, SQI reading turns normal to 7 and ethernet link is ok (ping good), no reset/power cycle happen
3. Hard to reproduce and only happen once after SOP
Regards,
Dongbao