Part Number: SN65HVD1050
Hi,
I observe that sometimes in the end of frame a high bit is present and I think the frame is not valid.
Other tmies this hig bit is preent in the acknolege bit, but hte frame is valid.
Someone could me tell me what is happends?
The system are three borads connected whit CAN bus by means of SN65HVD1050. The distance between boards are 10 cm.

is a valid frame

Invalid frame
I don't understand why this overvoltage is in the middel of the end of frame.
Thank you