Part Number: THVD4431
Hi Experts,
My customer wants to use RS232C and RS485((full-duplex mode). The termination resister can be enabled or disabled using pins. When setting TERM_TX = VIO and TERM_RX = VIO, the termination resister is enabled when RS-485 mode is enabled and disabled when RS232C mode is enabled. In other words, customer does not need to control TERM_TX pin and TERM_RX pin by external device to enable and disable the internal termination resister.
Is this understanding correct?
regards,
Uchikoshi