Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Help with MAX3232

Other Parts Discussed in Thread: MAX3232

Hi

 

I have a problem with a board with a MAX3232 device. What happens is if the MAX3232 is powered with a device (in this case a standard PC serialport) connected to the RX Input the charge pump doesn't appear to work. If you remove the connection and reconnect everything is fine and if you power the MAX3232 before connecting the PC everything is ok. It is only if there is -12V on the RX input when the MAX3232 is powered up that this happens. I have used these devices in plenty other designs over the years with no issues. On the board the MAX3232 is connected to a NXP LPC1752 Cortex-M3 processor.

 

Has anybody any idea of what could cause this behaviour?

 

Thanks

Ian

  • Hello Ian,

    This effect has not been reported before. Can you measure the voltages on the device pins when this anomaly occurs? Use an oscilloscope to see if there is any clocking. The pin voltages will be helpful in determining the root cause.

    Does this happen on more than one MAX3232 device? Is it a new design?

    Regards,
    Ron Michallick