This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDS1204: Is TMDS1204 possible to use 2560x1440p(30Hz) of Non-CEA format

Part Number: TMDS1204
Other Parts Discussed in Thread: TDP1204

Dear Specialists,

My customer is considering TMDS1204 and has a question.

I would be grateful if you could advise.

---

Is TMDS1204 possible to use 2560x1440p(30Hz)?

The required bandwidth is 6.18Gbps, so there is no problem.

Since this format is Non-CEA, I would like to check whether it can be used.

Is the answer the same for TDP1204?

---

I appreciate your great help in advance.

Best regards,

Shinichi