Part Number: DS90UB940N-Q1
Hi,
In our application, we encountered a problem where the video output was significantly delayed compared to audio. Upon some basic investigation, we noticed that the PASS & LOCK pin was LOW during the lack of video output. From the datasheet description of PASS, it could be potential corruption in the VS and DE timing.
My question is, without access to the serializer (video source) side, is there a way to check the timings of the VS and DE signal within the 940N deserializer?
Also since the PASS pin is flagged, is it right to say that the problem lies on the FPD-Link interface (input) and not on the CSI interface (output)?
Thanks in advance!