Other Parts Discussed in Thread: ALP
Hello,
I'm trying to connect a FPD3 camera to DS90UB940-Q1EVM and access the camera by I2C but this doesn't work for. The camera is the Allied Vision Alvium 1800 C-240C which is connected to J3 connector on the EVM (SMA connector). The configuration of the EVM is:
MODE_SEL0: 1 (4 data lanes, 1 CSI port active)
MODE_SEL1: 4 (HS Back Channel: 20 Mbps, Input Mode: Coax)
This is the current configuration of the registers:
Register Display - ALP Nano 1 - DS90UB940, Connector 1
Register Data Name
0x0000 0x58 I2C Device ID
0x0001 0x04 Reset
0x0002 0x00 General Configuration 0
0x0003 0xF8 General Configuration 1
0x0004 0xFE BCC Watchdog Control
0x0005 0x1E I2C Control 1
0x0006 0x00 I2C Control 2
0x0007 0x79 REMOTE ID
0x0008 0x78 SlaveID[0]
0x0009 0x00 SlaveID[1]
0x000A 0x00 SlaveID[2]
0x000B 0x00 SlaveID[3]
0x000C 0x00 SlaveID[4]
0x000D 0x00 SlaveID[5]
0x000E 0x00 SlaveID[6]
0x000F 0x00 SlaveID[7]
0x0010 0x78 SlaveAlias[0]
0x0011 0x00 SlaveAlias[1]
0x0012 0x00 SlaveAlias[2]
0x0013 0x00 SlaveAlias[3]
0x0014 0x00 SlaveAlias[4]
0x0015 0x00 SlaveAlias[5]
0x0016 0x00 SlaveAlias[6]
0x0017 0x00 SlaveAlias[7]
0x0018 0x00 MAILBOX_18
0x0019 0x01 MAILBOX_19
0x001A 0x00 GPIO[9] and Global GPIO Config
0x001B 0x00 Frequency Counter
0x001C 0x22 General Status
0x001D 0x60 GPIO0 Config
0x001E 0x00 GPIO1_2 Config
0x001F 0x00 GPIO_3 Config
0x0020 0x00 GPIO_5_6 Config
0x0021 0x00 GPIO_7_8 Config
0x0022 0x00 Datapath Control
0x0023 0x38 RX Mode Status
0x0024 0x08 BIST Control
0x0025 0x00 BIST ERROR COUNT
0x0026 0x83 SCL High Time
0x0027 0x84 SCL Low Time
0x0028 0x00 Datapath Control 2
0x0029 0x00 Reserved
0x002A 0x00 Reserved
0x002B 0x00 I2S Control
0x002C 0x00 Reserved
0x002D 0x00 Reserved
0x002E 0x00 PCLK Test Mode
0x002F 0x00 Reserved
0x0030 0x00 Reserved
0x0031 0x00 Reserved
0x0032 0x90 Reserved
0x0033 0x25 Reserved
0x0034 0x01 DUAL_RX_CTL
0x0035 0x00 AEQ TEST
0x0036 0x00 Reserved
0x0037 0xB8 MODE_SEL
0x0038 0x00 Reserved
0x0039 0x00 Reserved
0x003A 0x00 I2S_DIVSEL
0x003B 0x3F Reserved
0x003C 0x20 Reserved
0x003D 0xE0 Reserved
0x003E 0x23 Reserved
0x003F 0x00 Reserved
0x0040 0x43 Reserved
0x0041 0x03 LINK ERROR COUNT
0x0042 0x03 Reserved
0x0043 0x00 HSCC_CONTROL
0x0044 0x60 ADAPTIVE EQ BYPASS
0x0045 0x88 ADAPTIVE EQ MIN MAX
0x0046 0x00 Reserved
0x0047 0x00 Reserved
0x0048 0x0F Reserved
0x0049 0x00 Reserved
0x004A 0x00 Reserved
0x004B 0x08 Reserved
0x004C 0x00 Reserved
0x004D 0x00 Reserved
0x004E 0x63 Reserved
0x004F 0x00 Reserved
0x0050 0x03 Reserved
0x0051 0x10 Reserved
0x0052 0x00 areg12_2
0x0053 0x01 Reserved
0x0054 0x80 Reserved
0x0055 0x00 Reserved
0x0056 0x00 areg12_6
0x0057 0x00 areg12a_f
0x0059 0x7F Reserved
0x005A 0x20 Reserved
0x005B 0x20 Reserved
0x005C 0x00 Reserved
0x005D 0x00 Reserved
0x005F 0x00 Reserved
0x0060 0x00 Reserved
0x0061 0x00 Reserved
0x0062 0x00 Reserved
0x0063 0x00 Reserved
0x0064 0x10 PGCTL
0x0065 0x00 PGCFG
0x0066 0x00 PGIA
0x0067 0x00 PGID
0x0068 0x00 PGDBG
0x0069 0x00 PGTSTDAT
0x006A 0x00 CSICFG0
0x006B 0x00 CSICFG1
0x006C 0x00 CSIIA
0x006D 0x01 CSIID
0x006E 0x00 GPI Pin Status 1
0x006F 0x00 GPI Pin Status 2
0x0070 0x00 Reserved
0x0071 0x00 Reserved
0x0072 0x00 Reserved
0x0073 0x07 Reserved
0x0074 0x07 Reserved
0x0075 0x08 Reserved
0x0076 0x00 Reserved
0x0077 0x00 Reserved
0x0078 0x00 Reserved
0x0079 0x00 Reserved
0x007A 0x00 Reserved
0x007B 0x00 Reserved
0x007C 0x02 Reserved
0x0080 0x00 Reserved
0x0081 0x00 Reserved
0x0082 0x00 Reserved
0x0083 0x00 Reserved
0x0084 0x00 Reserved
0x0090 0x00 Reserved
0x0091 0x00 Reserved
0x0092 0x00 Reserved
0x0093 0x00 Reserved
0x0094 0x00 Reserved
0x0098 0x00 Reserved
0x0099 0x00 Reserved
0x009A 0x00 Reserved
0x009B 0x00 Reserved
0x009C 0x00 Reserved
0x009D 0x00 Reserved
0x009E 0x00 Reserved
0x009F 0x00 Reserved
0x00A1 0x00 Reserved
0x00A2 0x8C Reserved
0x00C0 0x00 Reserved
0x00C1 0x00 Reserved
0x00C4 0x00 Reserved
0x00C5 0x00 Reserved
0x00C8 0xC0 Reserved
0x00C9 0x00 Reserved
0x00CA 0x00 Reserved
0x00CB 0x00 Reserved
0x00CC 0x00 Reserved
0x00E0 0x00 Reserved
0x00E1 0x00 Reserved
0x00E2 0x00 Reserved
0x00E3 0x00 Reserved
0x00E8 0x00 Reserved
0x00E9 0x00 Reserved
0x00EA 0x00 Reserved
0x00F0 0x5F RX_ID0
0x00F1 0x55 RX_ID1
0x00F2 0x42 RX_ID2
0x00F3 0x39 RX_ID3
0x00F4 0x34 RX_ID4
0x00F5 0x30 RX_ID5
0x00F6 0x00 Reserved
0x00F8 0x00 Reserved
0x00F9 0x00 Reserved
And this is the information tab in ALP:
When I click on "Scan Connected Devices" I just see the EVM itself.
When I try to access the camera by I2C (e.g. reading out serial number at register address 0x198) it seems like the camera is not accessible:
board.ReadI2C(0x78, 0x198, 64)
[0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0]
Did I forget to configure anything to access the camera as an I2C slave?
Thanks,
Best regards.
Tanzou