Part Number: TUSB4041I
Other Parts Discussed in Thread: TUSB4041PAPEVM

The topology shown above is looking to be implemented. Are there any issues that arise when some ports support one speed and the others support another on the same HUB (2x HS and 2x FS in this case?)
The downstream devices will be streaming ~12kbps all the way up to 3000kbps or so. If the 12Mbps bandwidth of USB FS is to be shared between 6 devices downstream, are there any potential issues with limited speeds as well (if they really are streaming ~3000kbps.)
Please let me know if you have any other concerns with the topology as well.
Thank you
Matt