Part Number: ESD761
Other Parts Discussed in Thread: ESD751, TVS2700, TVS2200
Hi team,
Do we have ESD with 20V+ Vrwm and SOD964 package? Or could you recommend the most similar replacement? Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Kailun,
Unfortunately, we do not have a pin-to-pin replacement with a SOD964 package. We do have a leadless package with similar dimensions with the ESD751, which is a SOD523 (1.6mm x .08mm).
Do you have any more information on other requirements, such as channel count, clamping voltage, etc? TI offers many 20+ Vrwm devices, and more information will help us determine the best fit for your application.
Best Regards,
Josh Prushing
Hi Prushing,
Thanks for your reply. Our customer they have chosen a SOD964 product so they hope we could offer pin2pin product. This device is applied in fast charging type-C VBUS pin.
Hi Kailun,
Understood, thanks for sharing that information. Is there any way you could share the GPN/OPN of the competitor device they have chosen?
Best Regards,
Josh Prushing
Hi Kailun,
Understood on the competitor's name. Do you have any information on the specific device from Nexperia/Onsemi that is being used?
Best Regards,
Josh Prushing
Hi Kailun,
Please see the below comparison table for both devices. Unfortunately, we currently do not have any p2p options, but the green highlight designates a spec that the TI device meets or surpasses.
| Specifications: | PTVS26VZ1USK | TVS2700 |
| Vrwm (V) | 26 | 27 |
| Package Name | SOD964 | WSON |
| Package Size (mm) | 1.6 x 0.8 | 2.0 x 2.0 |
| Channel Count | 1 | 1 |
| Polarity | Uni-directional | Uni-directional |
| Clamping Voltage (V) | 38.4 | 33 |
| IO Capacitance | 215 | 100 |
| IEC 61000-4-2 Rating | 30 | 16 |
| IEC 61000-4-5 Rating | 32 | 40 |
| Max Leakage Current | 200 | 60 |
| Specifications: | PTVS22VZ1USK | TVS2200 |
| Vrwm (V) | 22 | 22 |
| Package Name | SOD964 | WSON |
| Package Size (mm) | 1.6 x 0.8 | 2.0 x 2.0 |
| Channel Count | 1 | 1 |
| Polarity | Uni-directional | Uni-directional |
| Clamping Voltage (V) | 33 | 27.75 |
| IO Capacitance | 247 | 105 |
| IEC 61000-4-2 Rating | 30 | 17 |
| IEC 61000-4-5 Rating | 37 | 40 |
| Max Leakage Current | 200 | 62 |
Please let me know if there are any additional questions!
Best Regards,
Josh Prushing
Hi Josh,
Thanks for you support! May I ask do we have similar size alternatives?
Hi Kailun,
Please see the table below:
|
This is our only +20V device in the 1.6 x 0.8mm package, but the TI device is leaded, as mentioned earlier in the thread. Below are the pictures of the layouts of each device:


Please let me know if you have any more questions!
Best Regards,
Josh Prushing