Part Number: DS90UH949-Q1EVM
Other Parts Discussed in Thread: ALP
Hello,
I have a 1920x720 display that is connected to a DS90UH948. By using the pattern generator on the 949, I am able to achieve a perfect image with the following settings:
Total Pixels: 2030 H, 731 V
Active Pixels: 1920 H, 720 V
Sync: 109 H, 10 V
Porch: 0 H, 0 V
However after plugging in HDMI, there is no image. Are there ways to internally change the registers to achieve an image? If there is no way on the 949 side, could I change registers on the 948 side to achieve an image?