This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCAN4550: CAN controller to support PeliCAN, just like SJA1000

Part Number: TCAN4550

Hi,

     my customer is searching a CAN solution which can support PeliCAN, just like SJA1000. any suggestions?

SJA1000:www.nxp.com/.../SJA1000.pdf;

  • Hello Ken,

    The TCAN4550-Q1 is the best option and has more features and configuration options than the SJA1000.  However it uses a different CAN Controller IP than the SJA1000 so it would not be directly software compatible.  However it should be able to accomplish the application related tasks if direct software compatibility is not required.

    Regards,

    Jonathan